RoHS & REACH
To our knowledge, our products supplied to you do not contain substances with concentrations that prohibit the placing on the market. The referred legislation is:
2011/65/EU - RoHS Directive
1907/2006/EC - REACH Regulation
2006/122/ECOF - Directive on restriction of perfluorooctane sulfonates („PFOS“)
1005/2009/EC - Regulation on substances that deplete the ozone layer
RoHS
Directive 2011/65/EU of the European Parliament and of the Council of 8 June 2011 on the restriction of the use of certain hazardous substances in electrical and electronic equipment
Directive 2011/65/EU (RoHS II) restricts the use of lead, cadmium, mercury, hexavalent chromium, polybrominated biphenyls (PBB) and polybrominated diphenyl-ethers (PBDE) in certain electrical and electronic equipment (EEE) since 3 January 2013. In July 2011, this Directive entered into force, replacing the old Directive 2006/95/EC (RoHS).
RoHS II has not added new substances to the list of restricted substances. However, the restrictions are no longer limited to the previous substances, but instead a process has been introduced to add additional substances in the future (similar to REACH).
Irrespective of the scope of the RoHS II Directive, all products in the main catalogue of the LAPP GROUP are in compliance with Directive 2011/65/EU on the restriction of the use of certain hazardous substances in electrical and electronic equipment (RoHS II). These products do not contain any of the restricted substances specified in the RoHS II Directive or exceed the maximum concentrations stipulated therein, except for the Annex III exemptions of this Directive.
REACH
Regulation (EC) No 1907/2006 of the European Parliament and of the Council of 18 December 2006 concerning the Registration, Evaluation, Authorisation and Restriction of Chemicals
With REACH, the European Community has created a harmonised System for the Registration, Evaluation, Authorisation and Restriction of chemicals. The goal is to ensure a high level of protection for the environment, health and safety.
REACH came into force on 1 June 2007 and replaced a number of former specifications relating to the material composition of products, as previously governed, for example, by directive 76/769/ EEC on the approximation of the laws, regulations and administrative provisions of the Member States relating to restrictions on the marketing and use of certain dangerous substances and preparations. All LAPP GROUP products are articles, not substances or preparations, as defined by REACH.
Here you can find a short overview about REACH and the statement of the LAPP GROUP.
For more information about REACH, please contact our REACH contact persons.