Broadband expansion
On-schedule site deliveries, reliable quality and immediate requirements for emergencies - these are the typical wishes of every civil engineering company. Our customers often lay fibre optic cables over long distances. In doing so, they try to avoid loss of performance. For future-proof broadband expansion.
With LAPP fibre optic cables, large amounts of data can be transmitted quickly and reliably. The data is transmitted as light signals. And that: metal-free, copper-free, interference-free and tap-proof. Even electromagnetic radiation does not affect the transmission.

Area-wide fibre optic connections are the precursor to a promising 5G infrastructure. LAPP sees this as an expansion of its current business segment "Industrial Communication". 5G technology is taking "Industrial Communication" to a new level of performance. Digital transformation and the massive increase in data traffic demand even greater network capacities. This is particularly true for the Internet of Things in industry and logistics. 5G has enormous potential to significantly improve machine-to-machine communication (M2M) in the automation of production lines - in addition, the high-performance radio standard provides stability in the mobile communication network. LAPP believes that 5G and other existing radio technologies are therefore an ideal complement to wired communication solutions.
COVID-19: Delivery times are durable, despite the current difficult situation
We know that broadband expansion in Germany is still in its infancy and each of your projects has its own challenges. Rest assured: we at LAPP are in the starting blocks. Together we will tackle the challenges and develop individual solutions that fit your needs. Our experts will be happy to advise you.
We are prepared: All common fibre optic cable types are in stock on maximum drum lengths for you to call up immediately. Thanks to our logistics processes, we can continue to offer you these products within Germany. So you can keep your deadlines despite the current difficult situation.
You need special fibres or lengths? We at LAPP can manufacture and test your desired length in the shortest possible time and deliver it to you worldwide.
Your advantages at a glance
- High availability from stock throughout Germany
- Delivery on rent-free solid wood drums on transport frame
- Customer-specific labelling options: Optimal allocation and theft-proof on your construction site
- Framework agreements with individual call-off cycles: Order once - call-off according to demand
- We offer all desired fiber standards, whether from production facilities in Europe or Asia
A record of all PCF results (verified by DEKRA) can be found here on this page and on the DEKRA CheckMe portal. Further information can be provided on request.
We believe that wireless and cables go hand in hand: 5G can only become reality with extensive broadband coverage. After all, the data is still transported to the radio masts using fibre optic cables. These therefore play a major role in the performance capability and reliability of the 5G network.
Powerful fibre optic cables represent the foundation of the digital infrastructure. With this in mind, we offer a broad portfolio of outstanding fibre optic cables to facilitate the fast and secure transfer of large volumes of data. LAPP also stocks PVC ground cables with copper conductors. These products are complemented by compatible connectors and SKINTOP® cable glands for a secure fit in next to no time. What’s more, our FLEXIMARK® labelling systems provide you with durable marking solutions that can still be easily read many years later.
Our fibre optic cables are characterised by exceptional fibre optic quality, meaning that large volumes of data can reach their destination quickly. Faults and outages constitute the greatest risk for broadband and 5G networks. In order to prevent these from happening, our cables are metal- and interference-free, with data transfer even immune to electromagnetic radiation. And as they frequently carry sensitive data, they also protect against interception.
We offer all desired fibre standards, which we manufacture at our sites in Europe and Asia. We are also able to develop individual solutions to meet your needs.
We support your infrastructure projects with our end-to-end management, aiding you from start to finish. Our project team has extensive experience with network infrastructure projects and will help you to implement them successfully. Benefit from our customised solutions for process optimisation!
Let our LAPP experts advise you
Whether it is a rewire that requires up to 288 fibres or an extension to the existing backbone network that needs two or more fibres, the LAPP is your expert solutions partner in all things related to cable and connection technology.
For your offer contact us via e-mail at SGP(at)lappkabel.de.
We only use top-quality glass fibres from prestigious manufacturers to meet our high demands on quality. Our products are being used in a range of applications, such as tunnel construction, industrial site networking and internal communication networks at energy suppliers.
A-D(ZN)2Y Fibre to the Home (FttH) Micro Cable
Micro special cable designed for installation by air-blowing systems (Micro Ducts).
Article List:
| Article designation | Tensile force N | Outer diameter (mm) |
|---|---|---|
| A-D(ZN)2Y 2 E9 / 125 | 80-100 | 2,6 |
| A-D(ZN)2Y 4 E9 / 125 | 80-100 | 2,6 |
| A-D(ZN)2Y 6 E9 / 125 | 80-100 | 2,6 |
| A-D(ZN)2Y 12 E9 / 125 | 80-100 | 2,6 |
| A-D(ZN)2Y 24 E9 / 125 | 80-100 | 3,0 |
| A-D(ZN)2Y 12 E9 / 125 | 100-300 | 3,9 |
| A-D(ZN)2Y 24 E9 / 125 | 100-300 | 4,0 |
Further designs and dimensions on request. Customized printing possible.
A-DQ(ZN)2Y with single-mode or multimode fibres. Mini outdoor cable designed for installation by air-blowing systems (Ducts).
Article List:
| Article designation | Tensile force N | Outer diameter (mm) |
|---|---|---|
| A-DQ(ZN)2Y 1x12 E9 / 125 | 1000-2000 | 5-6 |
| A-DQ(ZN)2Y 2x12 E9 / 125 | 1000-2000 | 5-6 |
| A-DQ(ZN)2Y 4x12 E9 / 125 | 1000-2000 | 5-6 |
| A-DQ(ZN)2Y 6x12 E9 / 125 | 1000-2000 | 5-6 |
| A-DQ(ZN)2Y 8x12 E9 / 125 | 1500-3000 | 6-7 |
| A-DQ(ZN)2Y 12x12 E9 / 125 | 1500-3000 | 7-9 |
| A-DQ(ZN)2Y 16x12 E9 / 125 | 1500-3000 | 8-10 |
| A-DQ(ZN)2Y 24x12 E9 / 125 | 1500-3000 | 9-11 |
Further designs and dimensions on request. Customized printing possible.
Outdoor cable with central loose tube and non-metallic strain relief, rodent protection, dielectric, UV-resistant longitudinally and laterally watertigh. Suitable for direct burial.
Article List:
| Article designation | Tensile force N | Outer diameter (mm) |
|---|---|---|
| A-DQ(ZN)B2Y 1x12 E9 / 125 | 3000-6700 | 8-10 |
| A-DQ(ZN)B2Y 2x12 E9 / 125 | 3000-6700 | 8-10 |
| A-DQ(ZN)B2Y 4x12 E9 / 125 | 3000-6700 | 8-10 |
| A-DQ(ZN)B2Y 6x12 E9 / 125 | 3000-6700 | 9-11 |
| A-DQ(ZN)B2Y 8x12 E9 / 125 | 3000-6700 | 10-12 |
| A-DQ(ZN)B2Y 12x12 E9 / 125 | 3000-6700 | 13-15 |
| A-DQ(ZN)B2Y 16x12 E9 / 125 | 3000-6700 | 14-16 |
| A-DQ(ZN)B2Y 24x12 E9 / 125 | 3000-6700 | 17-20 |
Further designs and dimensions on request. Customized printing possible.