Research & development

Images from our research and development departments for editorial publications about the Lapp Group.

Tip:
To save graphics formats that your browser can display directly (JPG, TIF, GIF etc.), right click and use the “Save Target As” function.

     
Endurance test plant, 55m effective length
(JPG 995 KB )
Endurance test plant for testing 55m high flexibility drag chain cables
Water protection category test
(JPG 461 KB )
SKINTOP® brass cable gland after a water protection category test in line with EN 60529
Fire test
(JPG 773 KB )
Testing the behaviour of cables in case of fire in line with IEC 60332.3